• LT3474 PWM dimming range

    Hi,

    The description of the page 1 of the datasheet shows 400:1 Dimming Range.
    However, the Dimming Control calculation example on page 16 shows a ratio of 300:1.
    Which is correct?

    Regards,
    HM

  • LT3474 in parallel

    Hi, 

    I'd like to use the LT3474 as a current source, but need max 3A, so I'm thinking of using them in parallel. How would you recommend to do that?

    Thanks for your help.

    Kind regards

  • LT3474 VADJ powered by DAC

    Hi,

    I was wondering if I can connect the VADJ pin directly to the output of a DAC. 

    Thank you,

  • LT3474 LED DRIVER

    I would like to purchase led drivers(LT3474) for my project(Visible light communication) which is capable of accepting a pwm signal from a microcontroller. I just have a few questions.
    1) How many LEDs in an array can I drive with a single led driver…
  • LT3474 SHDN pin control

    Hi, I want to use MCU pin to control SHDN pin of LT3474.

    As in the datasheet, I see the LT3474 doesn't have the internal pull down resistor so I must to use external resistor to pull down on the SHDN line, right?

    This is a discussion with my colleague…

  • RE: Lt3763 drive a 10A LD

    hi,i have a question about i want to drive a low power LD,maybe just have 100mA or 200mA,Can this chip accurately drive the laser? because in my mind ,LT3763 Suitable for driving high-power LED or LD,If not suitable for drive a low power LD,Can you recommend…

  • LT3474EFE#PBF Exposed Ground Pad

    We have a legacy design using a LT3474EFE#PBF where the exposed pad is not connected.  The data sheet indicates it is required to be connected to ground.  Will the device operate without the exposed pad connected to ground?

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032