• LT3462 How to use

    After simulating the LT3462 with the recommended circuit, there were no problems, so I mounted it on the board.
    When the input is set to 15V DC and the output is set to 18V,
    The output changes from about -19V to about -18.5V,
    A triangular waveform of several…

  • RE: How to use LT3464

    Your title says "How to use LT3464", and you are simulating the LT3462. Which one is it?

    Please state your input voltage range, and max load current.

    DV

  • RE: VIOC-Pin at the LT3094

    I don't consider myself a VIOC expert and I don't have any more time to spend on this, but this is my input:  Essentially, you need to level shift the VIOC output of your LT3094 to the VREF pin of your TI part.  The closest ADI part I have to check…

  • RE: Low noise negative votage

    LT3462/3462A for inverting DC/DC converter, followed by LT3090, could be considered.

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032