Good Morning ADI EnginnerZone community.
thanks for your support until now.
For medical qualification reason we need the MTBF/MTTF/FIT of LT3094.
But it is impossible to find the value or the process in
Good Morning ADI EnginnerZone community.
thanks for your support until now.
For medical qualification reason we need the MTBF/MTTF/FIT of LT3094.
But it is impossible to find the value or the process in
I am attempting to use the VIOC capability of the LT3094 to control an upstream LT8364, as shown:
This works as expected with little to no bypass capacitor on the LT3094 SET pin:
However, increasing the bypass cap (C7) to 100nF or more prevents the…
Please do SYNC RELEASE in LTspice. The model has been released. Thanks!
Best Regards,
Hong
The LT3045 datasheet clearly mentions reverse input protection, however I find nothing in the LT3094 datasheet.
Can a diode be inserted between the pins IN and PGFB of the LT3094 datasheet to provide such a protection, similarly to the LT3045 ?
I tried…
Hello
Customer request below dimension for layout footprint. Do we have these dimension to provide for layout? Thank you.
BR
Patrick
I have a design that uses two LT3045's and an LT3094, and most of these LDOs never work.
An LT3045 configured for 4.99V out (49.9k set resistor) typically sees 1.96V on the set pin. I have verified that the current source simply isn't working.…
Hello,
In the current application (symm voltages of LT3065 and LT3090 +/- 14V out output Cout 1000uF/ low ESR) , the LT3090 misbehaves during startup.
After recycling of input voltage, normal ops. I found this behaviour described in the LT3090 datasheet pg 21…