This EZ post may answer your question. The post title is "Disable LT3083".
This EZ post may answer your question. The post title is "Disable LT3083".
Hello,
I am using the LTC4015 with Solar Panels that have Open Circuit Voltage (Voc) as high as 42V, but the maximum voltage that can go into the LTC4015 is about 36V. So I am looking for a Voltage clamp / Regulator that can output 36V/3A from a 42V…
I am using an LT3083 as a 2-terminal current source, per the last figure in the data sheet. The LT Spice simulation works as expected, but the actual circuit has a residual voltage of over 2V when the set pin is grounded. I realize that there is a minimum…
Hi everyone
I am trying to design a VSSC circuit by LT 3083 to drive a LED or resistor . But the current is not stable as expected or described in datasheet by LT3083 . I tried to repalce the power with DC/DC or LDO ,but not improved .
Later ,I tri…
I just tried the LT1963-3.3 + LT3083 Boosting Fixed Output Regulators application from the image in my original post above. The circuit is also in the LT3083 datasheet. The output regulates correctly at no load and it was not necessary to add any preload…
各位大佬好:
小弟最近在使用LT3083设计一个功率较大(1A级别)的线性LED驱动器,方法是使用DAC输出参考电压Vref,连接到LT3083的Vset引脚,但是在测试时发现LT3083,当LT3083输出电流略大时(30mA),电流就十分不稳定。
测试条件简述如下:
1. 供电电源使用DC/DC 或者LDO时,二者测试效果无差别,电流波动大;
2. 负载使用水泥电阻 或 LED 时,二者测试效果无差别,电流波动大;
3. 参考电压Vref来源 : 使用DAC8563 或者NI 采集卡USB6009…
Hi Niels,
I can only find LT1084 that can support up to 5A. The LT3083 you asked in separate thread can only support up to 3A. The pass device is a BJT similar to LT3083 so I assume reverse leakage current you will expect may be similar.
I just asked the pcb designer for LT3083 demonstration circuit DC1585A and the pcb designer said we use a 0.004 inch to 0.005 inch thick stencil to apply the solder when we assemble the demonstration circuits. The LT3083 datasheet PACKAGE DESCRIPTION…
Hi Niels,
Thank you for your input.
1. output voltage controlled by a DAC
Yes, it can be controlled by placing DAC to drive the SET pin directly. I think a simple non-inverting amplifier powered by Vin will do the trick.
But I need…
The design group is responsible for the datasheet, but I asked the designer the same question about the similar LT3083 recently and the designer said in that case overload means that the device's current rating is exceeded. For instance, the LT3083…