• RE: LT3082 Set pin open

    I think your simulation results are correct.  I just opened SET on the LT3082 demonstration circuit with your conditions and the output voltage increased to VIN - VDROPOUT.

  • LT3082 Set Pin

    I'd like to use the LT3082 in a DAC controlled mode as shown in the typical applications section of the datasheet, but I'd like to do so without the gain stage shown. This should work as the op amp internal to the LT3082 has very high input impedance…

  • RE: 最近需要一款0-3.3V输入,4-20mA输出,3.3V或5V或12V供电的芯片,有什么好推荐的吗

    我想你應該是指定電流輸出吧???

    如果試的話  可以參考這顆LT3082 Datasheet and Product Info | Analog Devices

    或者是一般的linear type LED Driver

    在如果你是要定電壓  但輸出要有4-20mA 的話

    其實挑ADP12X 系列就很夠用了

  • RE: AD5270 stays in midscale

    The AD5270 is supplied with 5V (provided by a Zener Diode) on VDD and the VSS and GND Pins are connected to the board ground reference(DUT_S), as seen in the schematic below.

    The LT3082 sets a voltage on the output depending on the resistance between…

  • ARAD Supported Parts as of 2020 January 8_0

    adp1071
    adp1071-1
    adp1071-2
    lt1020
    lt1033
    lt1083
    lt1083-fixed
    lt1084
    lt1084-fixed
    lt1085
    lt1085-fixed
    lt1086
    lt1087
    lt1117
    lt1118
    lt1120
    lt1120a
    lt1121
    lt1123
    lt1129
    lt1175
    lt117a
    lt117ahv
    lt1185
    l…
  • RE: LT3090 output voltage controlled by DAC

    The image below shows the basic concept of how to control an LDO output using a DAC.  The LT3082 in the image is a positive LDO and the LT3090 that you want to use is a negative LDO, but it should still be possible to drive the LT3090 SET pin in a similar fashion…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • LT3080 Dropout Voltage

    A customer asks concerning the LT3080:  "We operate at: Vin = 3.3V Vout = 3V, Vcontrol = 5V, output current max. = 200mA. Is this ok?"

    This is a common question so I will answer it myself in a REPLY post.

  • LT3080 Exposed Pad Is Soldered to Ground by Mistake

    I get this question frequently so I will post the question and then answer myself:

    "I made a mistake and did not notice that the LT3080 datasheet says for the DD PACKAGE that "EXPOSED PAD (PIN 9) IS OUT, MUST BE SOLDERED TO PCB".  I made…

  • LT3081 SHUTDOWN - APPLIES TO MANY LT308X LDOS

    A customer essentially asks, "What is the easiest way to shutdown the LT3081 using a positive referenced logic signal?"  I get this question a lot so I will answer myself in a reply post.