• LT3071 Paralleling Devices

    Hi

    Are there any design examples (schematic and layout) exists for LT3071 load shearing with two LT3071 devices?

    Best Regards

    Alex

  • VIOS ,mode with LTC3416 and LT3071

    The LT3071 datasheet provides a good description of the VIOS mode and an sample design using this device with the LTC3415EUHF.  The LT3071 data sheet (page 17) says "It typically regulates the output of most LTC switching regulators or LTM power modules…

  • Fab process

    Hello, 

    I was wondering if you could provide the fab process used for the LTM4638 and LT3071 lines? I.e., CMOS, BiCMOS, GaAs, ect.

    Thank you 

  • LDO ADP1765 parallel for 1.8V/ 40A RF power application

    Hello,

    I want to use ADP1765 to deliver 1.8V/40A  RF power 

    Because of 1.8V/40A , it need 8 parallel

    Is this feasible?

    Or, do you have any concern , reference date or experience for this part?  

    BTW, is LT3071  suitable for this RF power application?

    thanks…

  • ARAD Supported Parts as of 2020 January 8_0

    adp1071
    adp1071-1
    adp1071-2
    lt1020
    lt1033
    lt1083
    lt1083-fixed
    lt1084
    lt1084-fixed
    lt1085
    lt1085-fixed
    lt1086
    lt1087
    lt1117
    lt1118
    lt1120
    lt1120a
    lt1121
    lt1123
    lt1129
    lt1175
    lt117a
    lt117ahv
    lt1185
    l…
  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • LT 3033 malfunctioning

    Hello,

    I am trying to test the IC : LT 3033. It has a linear regulator with a internal reference voltage of 0.2V. I had set feedback resistors of 150K and 11k to expect an output of 2.9V approx. However I am getting an output voltage of 0.48V at a supply…