• LT3050 output current limit

    I designed a LT3050 LDO with 5V in, 3.4Vout, 6mA Iout limit, 20kohm connected at Imon and Imax, Imin left float.

    The Imax can be measured to be at 600mV, the real output current (measured with an external ammmeter) was not limited to 6mA, but kept on…

  • LT3050: External current limit minimum value

    Hi

    I am trying to design a 15mA current limited 5V linear regulator. The input is 12V switching power supply (IRE-12/10-Q12PF-C).

    From the datasheet of LT3050, I could not tell if the part can be configured for a 15mA current limit. It seems that I(limit…

  • LT3050 Iout/Imon

    Hi,

    My customers are considering using the LT 3050.
    I got an inquiry there.

    The value of Iout / Imon was measured under the following conditions, and it was measured to be around 87 in actual measurement.

    Calculation using the calculation formula of…

  • RE: LT3063 load regulation

    Thanks for the post.  I will attempt to answer your question but I will also forward this post to the design group and I will post again if I am significantly corrected about anything.

    I think you are doing the load regulation calculation correctly and…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032