• LT3040 shutdown behavior

    Dear All,

    I have a doubt concerning the shutdown behavior of the LT3040.

    On page 21, in the power supply sequencing paragraph the datasheet says:

    If the VIN pin is powered high while LT3040 is in shutdown, the DC current flowing through the internal …

  • LT3040 output voltage up-scaling

    Hi all,

    The LT3040 has an input pin called V_FP. In all circuit schematics it is tied to the output directly. However according to the data sheet, this pin is only connected to the inverting input of the internal amplifier, so it would seem to me that…

  • RE: improving voltage reference noise performance

    Hi,

    Apologies, I know this is long overdue. However, we are clearing some open items and ensure that someone who have similar issue may find this helpful.

    First I am moving this to its proper community. https://ez.analog.com/analog-microcontrollers…

  • ARAD Supported Parts as of 2020 January 8_0

    adp1071
    adp1071-1
    adp1071-2
    lt1020
    lt1033
    lt1083
    lt1083-fixed
    lt1084
    lt1084-fixed
    lt1085
    lt1085-fixed
    lt1086
    lt1087
    lt1117
    lt1118
    lt1120
    lt1120a
    lt1121
    lt1123
    lt1129
    lt1175
    lt117a
    lt117ahv
    lt1185
    l…
  • 3-4月ADI新品主打,快来康康有没有适合你的设计~

    携一缕浅夏的芬芳,凝一脂冰清玉洁的清梦

    各位小伙伴们,迷人的仲夏五月来啦~

    在这个似水的季节里,悠然翻阅学习岂不美哉?

    今天斑竹给大家带来 ADI 3 - 4月的新品合集,想要了解学习的筒子可千万不能错过哦~

    MxFETM四通道 16 位 12GSPS RFDAC 和双通道 12 位 6GSPS RFADC AD9082

    发射信号前端 (MxFE®) 是一款高度集成的器件,具有 16 位、12 GSPS 最大采样率射频 (RF) 数模转换器 (DAC) 内核和 12 位、6 GSPS 采样率…

  • 在新年到来之际,送你一组钻石级硬度的精选硬核产品吧~

    转眼间,2020年就要结束了,今年你都做了些什么呢?

    对于ADI,我们可是推出了不少硬核产品哦~

    今天,斑竹就给大家晒晒ADI这些杠杠滴成果!

    -------------------------------------------------------------------------

    软件可配置的四通道输入/输出 AD74413R

    AD74413R是一款软件可配置的四通道输入/输出解决方案,适用于楼宇和过程控制应用。AD74413R包含用于模拟输出、模拟输入、数字输入、电阻温度检测器(RTD…

  • 2020年 ADI 20款硬核新品,为你献上电路设计的不二之选

    你最关注的领域是什么?ADC/DAC?Power?RF?.....

    你知道ADI在这些领域都推出了怎样的硬核新品吗?

    回首2020年,虽然被疫情干扰,不过咱ADI依旧没有停止推出新产品的脚步,今天斑竹就为大家盘点一下今年的“新秀”吧~

    四通道、软件可配置输入/输出 AD74412R/13R

    AD74412R 是一款适用于楼宇和过程控制应用的四通道软件可配置输入/输出解决方案。AD74412R 包含用于模拟输出、模拟输入、数字输入和电阻温度检测器 (RTD) 测量的功能,这些功能集成在一个单芯片解决方案中…