• LT3033 dropout voltage

    I am considering using the LT3033 because of it's low dropout voltage (95 to 135mV).   I have an input voltage in the range of 3.3 to 4.2v and my output voltage will be 3.1v.

    But I'm confused about note 4 on page 4 of the datasheet (https://www…

  • Maximum output capacitance for LT3033

    Hello,

    I am interested in using the LT3033 with up to 1.5mF of capacitance. I plan to achieve this output capacitance using a number of tantalum capacitors in parallel. Can the LT3033 handle an output capacitance this large? Will it cause the voltage…

  • LT3033 PG pin query

    Hi,

    Can the PG pin of LT3033 be left floating if it's not used? 

  • Is it acceptable to have LT3033 constantly running in drop-out mode?

    Hello,

    I'm interested in using LT3033 in a circuit I am designing, but my use case is a little unique, so I want to make sure I'm not misusing this part or exceeding any limits.

    I have a circuit that can accept voltage between 4.0 and 5.5V (consumes…

  • Voltage Input LT3033

    To obtain a voltage at the output of 3V3 and 3A, it would be possible to supply the LT3033 with a voltage of 3.5V or 3.6V. What would be the minimum voltage to have an output at 3V3 and 3A?

  • LT3033 absolute maximum rating

    Hi

    I have a question about SHDN_bar pin absolute maximum rating.

    Can we apply over VIN voltage to SHDN_bar pin ?(and Is there extra supply current?)

    Because we use under VIN=1.8V and SHDN_bar=5V logic.

    Best regards 

    Thank you very much.

  • No voltage regualtion of LT3033 after connecting load

    I was testing the voltage regulator LT3033. I have set the output voltage at 3.14V. But when I connect the load, I don't get the desired current. For example I connected a load of 10OHMS, I didn't get the exepected current. Also the output voltage would…

  • RE: LDO Regulators in Parallel

    LT3033 LTSpice model will be available soon. An example circuit using two LT3033s in parallel is shown on page 17 in LT3033 datasheet.

  • LT 3033 malfunctioning

    Hello,

    I am trying to test the IC : LT 3033. It has a linear regulator with a internal reference voltage of 0.2V. I had set feedback resistors of 150K and 11k to expect an output of 2.9V approx. However I am getting an output voltage of 0.48V at a supply…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032