Is it possible to use LT3032 in a floating design similar to LM317 and LM337 by using diodes? I need low current, low noise positive/negative voltage regulators which can work around 55V-60V region (both positive and negative inputs.)
Is it possible to use LT3032 in a floating design similar to LM317 and LM337 by using diodes? I need low current, low noise positive/negative voltage regulators which can work around 55V-60V region (both positive and negative inputs.)
Hello,
I downloaded the footprint of LT3032 from ADI WEB site. But, it is not for LT3032, I think. Because GND and INN are connected. Could you please check it and send me a correct footprint?
Best Regards,
Akira
Hi everyone,
I am trying to implement the LT3032 voltage regulator for the small footprint and low noise. However, in my current design I have the problem that the positive rail is oscillating with a frequency dependent on load current (a few kHz).
I am trying to use The LT3032 to generate dual outputs of +/- 4.4V. However, on the positive output I require 250mA and 100mA on the negative output. The datasheet says "Dual 150mA" and "Output current= +/- 150mA".
However LTSpice…
Hello,
I'm trying to use LT3032 in my design to regulate +/-15V supply voltages coming from DC/DC swithing regulator.
The output voltage of LT3032 is set to +/-14V with voltage setting resistors. However, output voltage is about +/-12V. I discovered…
Hi
I'd like to ask if there is LT3021 model available to be installed in ADIsimPE ? I know there is model available in LTspice, but the current project I am working on was built in ADIsimPE.
Best
Original Question: Is there a LT3032 model available for ADIsimPE ? by LuMA
Hi
I'd like to ask if there is LT2023 model available to be added in ADIsimPE ? I know there is a model in LTSpice, but the project I am working on was built in ADIsimPE ?…
Hi
I'd like to ask if there is model of LT3032 available to use in ADIsimPE ? I know there is a model in LTspice. But somehow the project I am working on is built in ADIsimPE
Best
The PCB files in .pdf can be found at https://www.analog.com/en/products/lt3032.html#product-evaluationkit. Save the DC1622A - Design Files and unzip it. All layout files, including the footprint, are in the DC1622A-pdf folder. Please let me know if you…
adp1071 |
adp1071-1 |
adp1071-2 |
lt1020 |
lt1033 |
lt1083 |
lt1083-fixed |
lt1084 |
lt1084-fixed |
lt1085 |
lt1085-fixed |
lt1086 |
lt1087 |
lt1117 |
lt1118 |
lt1120 |
lt1120a |
lt1121 |
lt1123 |
lt1129 |
lt1175 |
lt117a |
lt117ahv |
lt1185 |
l… |