• LT3022 output is false

    The output of LT3022 is designed to 0.85V as follows, but the actual output is 0.911V. Vin is 1.2V from DC-DC. If I remove the R889, the output of LT3022 is 1.143V and the volatge of ADJ is 0.268V.

    Then I design it in LTspice XVII and the output is same…

  • LDO芯片lt3022输出异常问题

    参考数据手册,选用LT3022可调电压输出模式。设计参数为,输入2.5V电压,根据手册配置电阻设计输出1V。

    但是实际测试电平为1.18V,当把输入电平2.5V换成1.2V时(其它配置不变)可以得到输出1V。

    请问出现上述现象是因为2.5V转1V的压降太大造成的吗?

  • ARAD Supported Parts as of 2020 January 8_0

    adp1071
    adp1071-1
    adp1071-2
    lt1020
    lt1033
    lt1083
    lt1083-fixed
    lt1084
    lt1084-fixed
    lt1085
    lt1085-fixed
    lt1086
    lt1087
    lt1117
    lt1118
    lt1120
    lt1120a
    lt1121
    lt1123
    lt1129
    lt1175
    lt117a
    lt117ahv
    lt1185
    l…
  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • LT 3033 malfunctioning

    Hello,

    I am trying to test the IC : LT 3033. It has a linear regulator with a internal reference voltage of 0.2V. I had set feedback resistors of 150K and 11k to expect an output of 2.9V approx. However I am getting an output voltage of 0.48V at a supply…