• RE: Use LT3010 to power LTC4020 INT_Vcc

    The LTC4020 datasheet says the INTVCC capacitor connects to PGND, so that is where I would ground the LT3010.

  • LT3010, LT3012 SHDN Timing

    I was considering using one of these linear regulators to power and LED.  I was wondering if the SHDN pin reacted fast enough to act as a PWM input at, say, 100Hz.

    Thanks,

    Dave

  • LT3010 or LT3014 internal reference temperature coeficient

    Hi,

    In datasheet of LT3010 or LT3014 is no data for internal reference temperature coeficient.

    Could I get this information?

    Thanks in advance!

    Best regards,

    Robert

  • 我使用的LT3010会出现容易坏的现象

    这是我的原理图,输入+48V电压,输出+25.6V,电流小于10mA,在使用中,或者存放一段时间,重新上电,

    就会出现输出电压不对的现象,请问各位大侠是什么原因?

  • 我使用的LT3010会出现容易坏的现象

    这是我的原理图,输入+48V电压,输出+25.6V,电流小于10mA,在使用中,或者存放一段时间,重新上电,

    就会出现输出电压不对的现象,请问各位大侠是什么原因?

  • LT3060 output capacitor 200uFx2

    Hello

            Customer use LT3060 (10Vin/3.3Vout). If add 220uFx2 on LT3060 output to supply MCU, the waveform is below and MCU damaged. It looks related to stability issue.  Could LT3060  or LT3010 output with 220uFx2? Has limitation of output capacitor? Thank…

  • ARAD Supported Parts as of 2020 January 8_0

    adp1071
    adp1071-1
    adp1071-2
    lt1020
    lt1033
    lt1083
    lt1083-fixed
    lt1084
    lt1084-fixed
    lt1085
    lt1085-fixed
    lt1086
    lt1087
    lt1117
    lt1118
    lt1120
    lt1120a
    lt1121
    lt1123
    lt1129
    lt1175
    lt117a
    lt117ahv
    lt1185
    l…
  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032