• Circuit design on LT3001

    Hello, dear colleagues!

    To clarify: my customer wants to design isolated power supply on flyback converter LT3001 (electrical principal scheme in attachment, transformer is 744889020330 by Wurth Elektronik), he made a board according to this scheme. He…

  • Special application with the LT8301 or LT3001 fly back converter

    LT8301.asc PDF

    I am building an application with the LT8301 or LT3001 fly back converter. I need four galvanically isolated 6V DC outputs with maximum of less than 5 mA capability. Attached is a LTSpice and a PDF file of the circuit. I have a prototype…

  • RE: Flyback isolated Controller

    Hi:

    The better option would be LT8301. If your application is not automotive, then the LT3001 is lower cost. Please contact your local ADI sales office for quote.

    Thank you!

  • 5V (USB) to 4-50V, 50mA isolated DC/DC converter

    We need  DC-DC converter which can generate a programmable voltage (via DAC or programmable potentimeter) in the range of 4V to 50V and 50mA. AND it has to be isolated with a few volt isolation - it only need to break a ground loop. It will be powered by…

  • ARAD Supported Parts as of 2020 January 8_0

    adp1071
    adp1071-1
    adp1071-2
    lt1020
    lt1033
    lt1083
    lt1083-fixed
    lt1084
    lt1084-fixed
    lt1085
    lt1085-fixed
    lt1086
    lt1087
    lt1117
    lt1118
    lt1120
    lt1120a
    lt1121
    lt1123
    lt1129
    lt1175
    lt117a
    lt117ahv
    lt1185
    l…
  • ADI 全新中文资料(2020 年 2 月)

  • C7 capacitance consultation in the middle of the isolation band

    Hello:

           I would like to consult the capacitor function of the middle C7 in the isolation band of DC3006A, and the design essentials that should be paid attention to if the isolation strength is 5000V. Do you have relevant design materials?