• RE: wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    Hello,

    sometimes page one of the datasheet contains the answer:

    The LT8708-1 always operates as a slave to the master LT8708 and has the capability of delivering as much cur-rent or power as the master.

    Hence I would state, that LT8708-1 can NOT work…

  • RE: For pin 1 orientation

    Hi Yatimun,

     According to the EIA spec 481-D, pin 1 should be in the first quadrant (upper left) if the user direction of feed is from left to right. You can find the link to this pdf on the data sheet itself at the bottom of page 2 *Tape and Reel LTC …

  • AD8195:  1:1 HDMI/DVI Buffer with Equalization

    Is there any documentation for the evaluation board for the AD8195?

    Thanks,
    John

  • Differential video transmission with ADA4433-1 and ADA4830-1

    Hello,


    Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).

    I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.

    The overall gain from input (ADA4433-1) to output (ADA4830…

  • RE: AD4110-1 ADC issue

    Hi Park,

    1. SYNC needs to be HIGH all the time for the correct operation of the device. The part will RESET modulator/digital blocks whenever SYNC is low. Hence, there is approx. 65.5MCLKS added to the settling time for the first conversion whenever SYNC…
  • RE: AD5755-1

    Hi Siva,

    You can use this: For Vout

    Vout = A*Vref * D*/(2^16) + B*Vref
    Where:
    A = FSR / Vref
    FSR = Upper output range - lower output range
    B = lower output range / Vref
    D = your code to the DAC register
    Vref = 5V

    ex. for +/-10V range
    FSR = 10 - (-10) = 20
    A …

  • How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…

  • Communication Issue between LTC6811-1 and LTC3300-1 via SPI

    Dear Colleagues from ADI,

    I've frustrated by this communication failure for quite long time, help from you is appreciated.

    SPI from LTC6811-1 can send out waveforms correctly and the code is as follow, but all two LTC3300-1 has no response(can’t…

  • (ADA4433-1) To connect ADA4433-1 to ADI Video decodor

    Hi !

    I have some questions about ADA4433-1.

    ******************************************************************************************

    Q1)

    Our customer are planing to make evaluation board to change "single-CVBS" to "Diff-CVBS" to input ADV7281A-M…

  • (ADV7390/1)Does ADV7390/1 supports ED-SDR 8bits 54MHz?

    Hi!

    I have some questions about ADV739*.

    (1)=========================================================

    I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.

    Does ADV7390/1 support that Video-format?

    Or must I use ADV7392/3?

    At the…