• LT1997-3 unused pins

    Sorry may be a trivial question...

    Using an LT1997-3 as differential amplifier with G=1 how connect unused pins ?

    thanks for help

  • LT1997-2 Distortion Specs

    Hello!

    In a LT1997-2 datasheet I see image on a page 1 with a THD spec on 1 kHz and on page 18 there is a Distortion section with a general words: "The LT1997-2 features excellent distortion performance when the internal op amp is operating in the normal…

  • LT1997-3 Rn、Rp Calculation

    Hello

    I tried to make a circuit equation like the attached file because I didn't know what to put as Rp, Rn to verify the formula of note 9 in the data sheet.

    Vos,out=(Vos x NOSEGAIN) + Ios x 22.5K + Ib x 22.5K x (1 - Rp/Rn)

    However, the above formula…

  • Behavior of LT1997(-3) in LTSpice

    I am evaluating an LT1997(-3) as a high-side current sense amp in a single-polarity system, up to 100+VDC.

    I modeled it in LTSpice, and am seeing unexpected results.

    The model doesn't seem to work with a single +5V supply, and gain configurations other…

  • wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    The LT8708EUHG-1#PBF specification shows that the LT8708-1 always operates as a slave to the master LT8708, Mainly used in parallel with LT8708, At present, our customer wants to use LT8708-1 (LT8708EUHG-1#PBF) separately without parallel connection.…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh