• LT1994 Temperature overheating

    Hello engineers

    Why the designed analog signal sampling circuit will cause the LT1994 to overheat,Can you give me some help?  

  • LT1994搭配LTC2385设计过热

    大神们好。设计了一款电路测试模拟信号,遇到LT1994温度过热,想寻求一下帮助。

  • LT1994 - Transient Analysis - LTSPICE

    Dear Support, 

    Error occurred "Analysis time step too small; time = 1.7562e-005, timestep = 1.25e-019; trouble with U5:swlim-instance s:u5:4"  while doing transient analysis with LT1994 .Please guide me to sort out this issue. 

    Figure1: Time step…

  • LT1994 Bandwidth

    Hi

    My customers are considering LT1994 and received questions about bandwidth.

    <conditions>
    Input signal: ± 1 V
    Gain: × 4

    #1   What is the bandwidth at this time?
           Considering from GBP (70 MHz) when Vs = 3 V,
           Is it about 70 ÷ 4 = 17.5 MHz?

    Best…

  • VOCM in LT1994 LTspice model is not working

    Pin VOCM in LT1994 is not works, it is totally work in wrong way. please correct it. :'(((((((((( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'( :'(…

  • RE: AN-159 LNA BOARD NOT WORKING

    Hi Erkan,

    Apologies for the late reply. 

    I took a look at your snapshots and saw some LT1994 units had wrong orientation. This is likely the cause of the board not working as expected.

    In parallel, we'll work on fixing the mask issues on the board to properly…

  • Amplifiers power consumption ambiguity

    In LT1994 by 150 diff load and 3.3 single supply yo can see this:

    At the right side of picture you see "power". It says 23.1mA into Vcc! and 18.8mA from Vee!

    First OpAmp must sink current from Vcc not sourcing to it!!!! secound why these (from…

  • RE: I am designing a circuit for driving a differential input ADC. As operational amplifier I use LTC 6254. My design works fine when simulating in LT Spice. However, when it comes to analyzing one of my outputs using a spectrum analyzer voltage level...

    Yes my input signal is always below 5MHz.
    I have looked through the differential amplifiers you suggested  AD8139,    LTC6404-1,  ADA4940,  LT1994.
     
    One other requirement in my design is that the input source is a high impedance…
  • Application Note 159: Measuring 2nV/√Hz Noise and 120dB Supply Rejection on Linear Regulators

    Hello, I have some questions regarding the low noise and high PSRR circuit design described in Application Note 159, AN159: Measuring 2nV/√Hz Noise and 120dB Supply Rejection
    on Linear Regulators.

    I would like to build the circuit in figure 16 on…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…