• 4:4:4 encoding?

    Is there an Analog Devices part that can accept 4:4:4 encoding?

  • ADV7612 4:4:4 YCrCb

    Hi

    datasheet on page 13 states that the ADV7612 supports 36-bit 4:4:4 YCrCb, but the table 5 and 6 do not list this mode. Is it supported, how can it be activated?

    best regards


    Dani

  • av code section for 4:4:4

    I have a question. What is the content of Section AV for YCbCr 4:4:4 24 bit interface?

  • ADV7612 DDR 4:4:4 Output Modes data

    Page 13 of DS describes the PIXEL INPUT/OUTPUT FORMATTING The output section of the ADV7612 is highly flexible. The pixel output bus can support up to 36-bit 4:4:4 YCrCb or 36-bit 4:4:4 RGB. The pixel data supports both single and double data rates modes1…

  • ADV7619 4k 8bit 4/4/4 pass through

    Hello,

      I wanted to ask for clarification on the VS and HS signals with the ADV7619 in pass through mode.  i read the thread on this previously https://ez.analog.com/message/156902#156902 and it does say that the CP will be bypassed and the syncs remain…

  • ADV7627 RGB 4:4:4 Color Space Issue

    We are using the ADV7627.

    An error occurs when we have a source generating RGB 4:4:4. Output color is incorrect and exhibits lots of pink.  When the source is connected directly to the display everything looks just fine. BTW, auto-CSC doesn't seem to…

  • ADV7511 1080p RGB 4:4:4 script needed

    Could you please provide the IIC configuration script for ADV7511 HDMI

    I am working on the ADV7511 chip, which is the HDMI codec in VC707 EVB from

    FPGA company Xilinx.

    I want to configured the ADV7511 working in 1080P, 4:4:4 RGB input (each

    component…

  • ADV7625 RGB 4:4:4 Color Space Issue

    I started this question with my original post: ADV7627 RGB 4:4:4 Color Space Issue 

    Colorspace continues to plague my system and I am looking for some guidance. I have spent a considerable amount of time looking at the AVIAPI routines but there are some…

  • Any SDTV Video Decoder with 4:4:4 output?

    Hi we are looking for a video decoder which can convert PAL/NTSC composite, S-Video and YPrPb.
    Output format doesn't matter, it can be YCrCb 4:4:4 or RGB (it will go to FPGA so we can do any conversion).
    However all SDTV decoders I found only produce…

  • ADV7181B RGB 4:4:4 640 x 480i configuration

    To digitize RGB, 4:4:4, 640 x 480i, square pixel video at a 30Hz frame rate please confirm the following.

     

    ·         Need a 28.63636MHz, < 50ppm crystal

    ·         Table 21 in the user manual shows NTSC square pixel format is supported. Is the square pixel format…