• PSSR Ratios of Following Devices

    Hello to all!

    I'm an electrican engineering student and working on a PSU at the moment. It's gonna be used on the electrical music instruments. So i need to eleminate all the noise and ripple at the output as much as possible. After switching sources…

  • RE: RH1965 Power Supply Ripple Rejection (over varying frequency)

    We don't have the data specially for RH1965, but you can use the PSRR of LT1965 as the reference. The bandwidth of RH1965 is lower than that of LT1965, so please add more output capacitance at high frequencies.

    LT3042 has ultrahigh PSRR. I would recommend…

  • RE: 发烧友不容错过丨高性能音频系统的两个关键器件

    ADI出色的LDO产品,最适合高分辨率和高质量产品,想了解就拿走~

    LT1763产品详情:https://www.analog.com/cn/products/lt1763.html

    LT1964产品详情:https://www.analog.com/cn/products/lt1964.html

    LT1965产品详情:https://www.analog.com/cn/products/lt1965.html

    LT3015产品详情:https://www.analog.com/cn/products…

  • Buck or LDO

    Hello team,

    I am rather confuse on my selection of using LDO or using buck.

    My power input range from10.8V-13V and I require a regulated  output of 10V and 1.2A.

    I am currently looking at LTM8074 and LT1965.

    Which would be more suitable for my use? I am…

  • ADP5071使用问题

    想要设计一个单电源12V输入,±电源输出(±13V)的电路,设计参考了ADP5071的Demo设计(UG484文档),

    在项目中真实采用了ADP5071+LT1965+LT3015的3颗物料,组成如下所示的电路,

     ,±13V后续所接的负载为30颗双运放OPA器件和8颗仪表运放器件,根据手册数据来看,OPA的典型静态电流为1.2mA,仪表运放的静态电流为2mA,因此计算的功耗预估为1.2x2x30+2x8 = 88mA。

    在实际电路调试过程中,碰到如下所述问题…

  • Two Crucial Components for Your High Performance Audio Systems

    High resolution, high fidelity and high quality are some typical jargon used in the audio industry, but they truly are essential features for an audiophile. Whilst they look so attractive, they are not so easy to achieve unless the right components…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032