• RE: Clock distribution of ultra low noise OCXO

    Dan, 

    Thanks.  The LTC6955 is a stripped down version of the LTC6953.  We basically just disabled some circuits on the LTC6953 to make the LTC6955..  The LTC6955 will be the same or better than the LTC6953 in all cases.

    I've been meaning to look at the LT3045…

  • RE: About LT1963ES8(ajustable LDO) application

    May I see the output voltage waveform during power-on? What is the peak voltage?

    The ADJ pin voltage is 1.21V when the output is regulated. Did you take the part off the board when you measured the voltage drop from ADJ to GND, and vice versa for used…

  • ARAD Supported Parts as of 2020 January 8_0

    adp1071
    adp1071-1
    adp1071-2
    lt1020
    lt1033
    lt1083
    lt1083-fixed
    lt1084
    lt1084-fixed
    lt1085
    lt1085-fixed
    lt1086
    lt1087
    lt1117
    lt1118
    lt1120
    lt1120a
    lt1121
    lt1123
    lt1129
    lt1175
    lt117a
    lt117ahv
    lt1185
    l…
  • RE: LT3081 floating reg as battery charger?

    OK, guess, I'll go it alone on this - looking into the online problems with these parts, such as LT3080, it might be best for me to steer away from LT308X parts. Pity as they held some promise.

    But before I completely give up on LT308X parts maybe…

  • LT1963AES8-3.3

    各位专家:

            我在使用LTLT1963AES8-3.3芯片时,遇到如下问题。电路的目的是通过STM32 MCU单片机的I/O控制LTLT1963AES8-3.3的SHUT 管脚,STM32 MCU单片机的I/O (PSW_1)配置成开漏输出,内部无上拉,外部接1M的上拉电阻,当PSW_1为1时,可输出LTLT1963AES8-3.3可输出3.3V电平,当PSW_1为0时,LTLT1963AES8-3.3可输出不是0V,而是1.4V,找不到原因。请帮分析下,电路图如下:

  • About thermal resistance of LT1963ES8

    Hi,

    I need the following information of LT1963ES8 : θJC & ψJT

    Would you please provide the information.

    Best Regards,

    mochi

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032