• LT1963 / LT3015

    Hello,

    I would like to know if there is a maximum limit to the bypass capacitor (CFF).

    In my simulator it also plays a role in the output impedance (low frequencies), I came up to 47µF !

    The LT3015 Data sheet says : CFF ≥ 10 nF/100µA • IFB-DIVI…

  • Difference between LT1963A and LT1963 ?

    Hi there,

    What is the difference between LT1963A and LT1963 ? Thanks!

  • RE: LT3083 as current booster

    You can use any LDO you like to replace the LT1963-3.3.  The 33k is just a 1mA preload as far as I can tell.  The LT1963-3.3 can supply 1.5A maximum, and the LT3083 will supply twice the LT1963-3.3 current due to the 20mOhm to 10mOhm ratio.

  • HMC7043 Power supply regulator design with HMC7043 EVM board.

    Dear Experts,

    My customer is making the power supply regulator design for HMC7043. Could you please reply to the following questions?

    Q1: The HMC7043 EVM board uses LT1963 for 3.3[V] power supplies of HMC7043. According to LT1963 datasheet, the maximum…

  • RE: LT1963AES8-3.3

    Can you disconnect the load from LT1963? When PSW_1 is 0, are there any other circuits running in the system to make the output of LT1963 pulled to 1.4V?

  • RE: Pass element LT1764A and LT1963A

    Both LT1764A and LT1963 use PNP as the pass element.

  • RE: LDO 充電器

    ADI收购了凌特,凌特的LT1963电源芯片应该能满足要求

  • RE: Powerful 的大咖现身,有奖邀你来谈 Power

    ADI+Linear的合体堪称完美,正如它说一样1+1>2!在工作中接触电源模块也多像LT1963、LT1764等这样的模块,在实际工程应用非常多,屡试不爽。

  • RE: LT3081 and LT3083 Application Examples - Boosting Fixed Output Regulators

    I just tried the LT1963-3.3 + LT3083 Boosting Fixed Output Regulators application from the image in my original post above.  The circuit is also in the LT3083 datasheet.  The output regulates correctly at no load and it was not necessary to add any preload…

  • RE: AD9779A close in noise

    Hi, All!

    I have a custom board with an AD9779A. The DAC is clocked from a VCXO 80MHz AT-cut level 3-rd overtone with PLL frequency multiplication inside the DAC and a final frequency of 320MHz. For analog power, I used an LDO LT1963, which has noise below…