• LT1935

     When my input the voltage to 10V, the IC does not work. Can anybody think of a practical way out of this situation?

  • LT1935升压问题

    使用LT1935电路,当输入5V时,能正常输出12V。

    但是当输入电压达到11V时,输出电压就稳不住,没有升压,输出比输入电压还低。

    有办法解决吗?

  • LT1930 Dual Output Converter Topology

    Hi,

    I notice that LT1930 has a special output circuit (datasheet P8).

    How can I calculate the valus as Vin, L1, Iout, Vout, C1 and C2 if I want to change them?

    For instance, I need 12V input while dual 18V ouputs.

    It seems that…

  • RE: Please analyze this circuit of LT1613

    Hi Kevin,

    Thanks again. I am studying LT1935 and LT8335, both have more than 2A switching current.

    Best Regards.

  • LT3652 & SEPIC

    Hi - I have a design with the LT3652, it's a very good chip. I'd like to know if there is chance that it could be used in a SEPIC topology? I use it as a 3-LiIon charger (1A), but my Vcc can be from 10 to 20V. So currently, I have a LT1935 to do…

  • Comparison of two dual +-V output converter circuist: LT1930 vs LT8335

    Hi,

    I am studying on dual ouput converter based on SEPIC topology. I find from datasheets that both LT1930 and LT8335 could create a symmetrical dual output. Please see.

    The pictures show clear that there are 2 kinds of circuts to create dual +-V outputs…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032