• LT1933 SOT23 package dimension

    Dear Sir /  Madam,

    I found that LT1933 SOT23 LTC DWG doc is different from ADI standard SOT23 LTC DWG.

    In LT1933 datasheet, SOT23 LTC DWG is 05-08-1634. However,  ADI standard SOT23 LTC DWG 05-08-1636

    2 drawing has different in dimension range.

    Could you…

  • Get symetrical voltage +5V;-5V using double LT1933?

    Hello,

    I would like to use 2 LT1933 to get symetrical voltage using single power supply 32V.

    Please tell me if below connection is acceptable:

    Using simulation shows correct output:

    7652.Draft1.asc

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • LT3470A

     PDFHi,

    I am Facing one problem with module LT3470A.

    This module configured as buck converter which will give 2V constant output at input range of 6V to 20V.(load less than 50mA)

    As per the data sheet pins are configured. This is my typical design.(Here…

  • ADV7180 & ADV7173 Interconnect Problems

    For a project in which I wanted to test the video decoding abilities of the ADV7180 by sending the digital video to a video decoding chip, ADV7173.

    My setup consists of the basic setup in the ADV7180 datasheet (pg 107 - Mode 1 CVBS Input (Composite Video…