• The gm of error amplifier used in LT1931

    Hello I am trying to simulate the block diagram of LT1931.here some of the values like transconductance of error amplifier is not clear.not able to simulate the block diagram of LT1931 because of the less imformation in the block diagram.so can anyone…

  • LT1931 maximum working voltage

    IN LT1931 datasheet, it says its maximum operating voltage is 16V. In the meanwhile, its absolute maximum Vin is also 16V. My question is if this LT1931 can work with input voltage 16V? Thanks. 

  • absolute maximum negative voltage of VIN for the LT1931

    Hello,

    What is the absolute maximum negative voltage of VIN for the LT1931?

    I think it's -0.3V instead of 0V.

    Best Regards,

  • About LT1931 power output NG

       HI.  

       I uses negative power output IC LT1931ES5.

       Previously, the device had no problems. 

       But, The LT1931 purchased this time can not a voltage trigger.

       As soon as the negative voltage is initially output, it drops to 0v.

       I bought it an authorized…

  • RE: Voltage inverter for LT3482

    Hi,

    there are many other parts dedicated to producing negative voltages, such as LT1931, LT3483, and others.

    LT8331, LT8361, LT8365 and LT8362.can generate, and regulate either, positive or negative.

    Depending on your requirements, one of those should…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032