• LT1930 Dual Output Converter Topology

    Hi,

    I notice that LT1930 has a special output circuit (datasheet P8).

    How can I calculate the valus as Vin, L1, Iout, Vout, C1 and C2 if I want to change them?

    For instance, I need 12V input while dual 18V ouputs.

    It seems that…

  • Comparison of two dual +-V output converter circuist: LT1930 vs LT8335

    Hi,

    I am studying on dual ouput converter based on SEPIC topology. I find from datasheets that both LT1930 and LT8335 could create a symmetrical dual output. Please see.

    The pictures show clear that there are 2 kinds of circuts to create dual +-V outputs…

  • RE: LT8471 - Dual +-12V Converter - Calculation

    Greetings Markus,

    Thank you foe pointing me out.

    Would you please explain more about that SEPIC dual +- output? In this circuit of LT8335, can I replace L1B and L1C with 2 Schottly diodes? Just like the circuit of LT1930 in the datasheet on the end of…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • The gm of error amplifier used in LT1931

    Hello I am trying to simulate the block diagram of LT1931.here some of the values like transconductance of error amplifier is not clear.not able to simulate the block diagram of LT1931 because of the less imformation in the block diagram.so can anyone…