• LT1819 not responding

    In simulation LT1819 is working at -3V to +9V, but in actual is not working. Another issue is if I connect 0 to 5V also It is not responding. Can you please help on this

  • LT1819 is supplied by +-5V when it works with LT2310 as ADC drivers ?

    the first question:In the reference SCH DC2425A,LT1819 is supplied by +6/-6v. Is it ok if the chip is supplied by +5/-5V? In the datasheet, it says Specifi ed at ±5V, Single 5V Supplies, why it supplied by +6/-6V?

    the second question, the following…

  • RE: LT6203 as Buffer Amplifier

    Hello,

    For the LT6203;
    The BufferP and BufferP-to-BufferN are measured values.
    Is the IN+ value is also a measured value? or this is the set value of your external supply?

    If the IN+ value is a measured value, please try to configure your LT6203 into single…

  • RE: Power Supply Modulator

    Hi Hari,

    Unfortunately we do not support TI products here on Engineerzone. Can you tell us more about your systems specifications so we can suggest an analog part that suits your need.

    You may want to check LT1819, ADA4857 or LT6411 as a start.

    Regards,

  • Serial to parallel LTC2325 cannot get the correct waveform

     The amplifier I didn't use the recommended LT1819, I used ADA4927-2, may be the reason is incompatibility.

    I used signal generator to input sine wave(100MHz, Vmax=1V, Vmin=0V), but I cannot get the correct waveform from the function "set up debug…

  • RE: about AD828 Video OPAMP

    Assuming you need a closed loop gain of 2 or thereabouts, you could look at the AD8002, AD8008, AD8056, AD8062, EL2260, LT1819, MAX4216 or OPA2658.

    ICs do not get discontinued in a First-In-Last-Out way, so you can't be sure that an old device like the…

  • LTC2323-16 Temperature dependent spikes in the output signal at negative half wave)

    Hi,

    the LTC2323H is used in our design which has an operating temperature range from -40°C to 125°C.

    The problem with our design is that "spikes" show up as soon as a temperature of ~65°C is increased (inside a thermal chamber).

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • RE: Video DACs ADV7123-EP and ADV7393 output opamp driver circuit

    Attached is a app note on general video circuits including AC-coupling

      PDF

    For full galvanic isolation might be accomplished using video transformers however I do not have any experience with this path.  There are several transformer solutions used in…