• LT1683 (DC477A) Closing the loop

    Hello,

    I am currently in a design which involved LT1683.

    I have checked the design of demo board DC477A which uses LT1683. 

    I have implemented it but using my design parameters (48V - 24V@100W) but the behavior is not OK, even after simulation on LTSpice…

  • LT1683 strange behavior on gate drive

    Hello I'm develop

    a low noise push-pull with LT1683.

    I observe that when voltage on CS pin 4

    go over 100mV, LT1683 turns on GATE-A and GATE-B simultaneously

    causing short circuit.

    Vin and GCL are tight together at 15Volt.

    I use 5pF to CAP-A, CAP…

  • RE: Push pull with unbalanced outputs

    ah :-) ok, you are right !! ... LT1683

  • Do ADI offer a low noise push-pull driver?

    I'm considering using one of the Linear Technology push-pull driver chips, e.g. LT1533, LT1683 or LT3439. At over $4 they are pretty pricey, so I'm looking for alternatives. Do ADI have anything equivalent?

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032