• LT1677 (NC) pin connection

    Hello,

    I would like to use NC pin.5 of LT1677 for a guard ring (tied to Vin-). In data sheet this pin is marked as NC, but

    it is not clear if this pin is floating or in some way tied to die. This will help me with more optimal routing , since I 

    have very…

  • LT1677-AMPLIFIER O/P LOOKS WEIRED

    Dear Team,

    I am developing a circuit which will convert a DC value of 2.8V to a square wave of value 2.8V and 3.3V. This is done by using an opamp as an amplifier and a transistor is used to as a switch to do this.But I can see output is not proper and…

  • RE: URGENT DATA REQUEST FROM FLEX FOR PART NUMBER LT1677IS8#TRMPBF

    Hello Siddesh,

    Here is the datasheet link: LT1677
    As for the other inquiries, we cannot answer them through EngineerZone but I believe they are already being handled offline.

    "We do not provide information regarding part markings on EngineerZone. We…

  • RE: Low noise adjustable reference for 24-bit audio R2R DAC

    Thanks Mon,

    I understand. I want use solution with pasive filtration and buffer. But recommended op's have low supply voltage. Can you recommanded somethimg elese? Maybe LT1677?

    Thanks

    Jan

  • Recommend me low-voltage dynamic microphone preamp circuit?

    Can anyone recommend me low-voltage dynamic microphone preamp circuit similar to this one for ECM http://www.analog.com/en/products/amplifiers/operational-amplifiers/high-voltage-op-amps-greaterthanequalto-12v/lt1677.html#product-overview ???

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • OPAMP lt6200-5

    In LT6200-5 OPAMP datasheet it is given that gain bandwidth product is equal to 800MHz at Av>=5. What is the maximum frequency at which LT6200-5 can be operated  with proper rise and fall time.?

    Is there is any method to improve the rise and fall time…