• LT1881 vs LT1636 dynamic load

    Using the LT1881 as the difference amplifier for a dynamic load.

    The output of the Opamp is slammed against the positive rail regardless of the value of Vctrl.

    If I simulate the same circuit using an LT1636, like I saw in someone else's design, and the…

  • RE: Ltm8055 parallel

    Since you are not using Rsense, try to copy the example on page 21 instead. Try removing LT1636 for now to be able to copy the example on page 20.

    Regards,

    Jhun

  • Two LTM8055 Peripheral circuit

    Hi,

    My customers are thinking about using two LTM 8055.

    Therefore, They decided to draw a circuit by the composition of data sheet P.20.
    There is a LT1636 between the two LTM 8055.

    #1  In the case of the circuit configuration shown below, is there a detailed…

  • RE: LTM8055 Parallel Operation

    Hi, here's the result of the startup test of LTM8055 in parallel configuration with 24V input (Blue), 12V output (pink), and 12A load (green). The result shows unnoticeable overshoot in the output voltage. 

    Take note that I have used two DC2017A evaluation…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • LT8490 charging will not initiate

    Hello,

    Problem: LT8490 is not initiating charging stages. It has a status code, and some SVRO pins that go high signifying an error. I designed the whole thing. Ask me anything.

    Input Max = 52V, 35A

    Output Max = 42.6V, 30A

    I had an old board revision that…