• +-5 from single +5

    can you suggest any way to produce +-5 from +5.
    I need it for one 4ch differential signal summer op-amp plus salen-key filter op-amp.

    Is there any DC/DC converter or something in ADI that doing this?

  • VDK Messaging Loopback with Node to Node Messages (BF561 VDSP 5 Update 5)

    I am trying to understand how the use of loopback (option 1 in the attachment) works when utilizing node to node messaging.

    It is my understanding that in loopback all messages would be created upon initialization and the messages are reused as needed…

  • About LT8619IMSE-5#TRPBF

    Hello,

    We use LT8619IMSE-5#TRPBF in our design to convert 24VDC to 5VDC.

    Here is our schematic:

    The problem is that the IC is broken and especially Vin and EN0UV pins have burned.

    The output current is about 200mA, switching frequency is about 500kHz…

  • RE: LTM8055 EVB Vout= 24V, from Vin=5-36V for 5A

    Hello Carmen,

    50W in general are not an issue, you just have to check if Vin/In respective Vout/Iout combination are within LTM8055 spec.
    Example: 48V@1,04A -> will not work as 36V Vout,max
    Example: 5V@10A, will not work as Iout has a smaller limit…

  • accel_ifft_large ERROR 5

    Hello,

    I am receiving an error from accel_ifft_large function with the error handler print:

    once:

    "ERROR: FFT error code 7"

    and then I receive a lot:

    "ERROR: FFT error code 5"

    Where can I see the documentation of and information about…

  • RE: ADN4654/5 for DisplayPort

    Hi Ray,

    I would recommend using some video conversion to send the video stream through multiple ADN4654; as the ADN4654 is limited to 1.1 Gbps, while DisplayPort requires 1.62 Gbps minimum.

    Also DisplayPort would require the control data to be isolated…

  • AD7091R-5 I2C

    Hi

    I'm a DFAE in Japan. Our customer give us a question. There is a MOSFET inside SDA pin of AD7091R-5. On the other hand, is there NO MOSFET inside SCL pin of AD7091R-5? According to Table 5, we couldn't see Open-drain output about SCL as follows.…

  • OPAMP lt6200-5

    In LT6200-5 OPAMP datasheet it is given that gain bandwidth product is equal to 800MHz at Av>=5. What is the maximum frequency at which LT6200-5 can be operated  with proper rise and fall time.?

    Is there is any method to improve the rise and fall time…

  • RE: LT6600-5 Gain Profile

    The LT6600-5 at 18dB passband gain will have a peak gain around 5MHz higher than the 18dB at lower frequencies.

    The LTspice model is not adequate for high gains because the simple model amplifiers do not show the limits of the IC amplifiers.

    At 12dB or…

  • LT1019-5 DIP8

    关于LT1019-5 DIP8 是否有可替代的料