Dear all,
请问可以使用LT1185产生-15V、3A的负电压吗?
如果可以的话,输入电压范围是多少?
该状态下,LT1185温升有多少,大概要选择多大的散热片进行散热?
非常感谢!!
Best regards!
Dear all,
请问可以使用LT1185产生-15V、3A的负电压吗?
如果可以的话,输入电压范围是多少?
该状态下,LT1185温升有多少,大概要选择多大的散热片进行散热?
非常感谢!!
Best regards!
Dear sir or madam
I'm confused about how to design a positive output with LT1185 as it mentioned in its datasheet .
I've already had a DCDC ,(LTM4622A), which generates both 8.5V(adjustable) and 3.5V(adjustable) . Now , I'm going to insert a LDO…
Dear sir or madam
I would like to inquire about the design of the LT1185 device.
As shown in the diagram I attached below, I currently have two LT1185s and are designing a circuit for positive output and negative output power.
The design of a positive output…
Hello,
Is there a spice model for the RH1185AMK? If not, is the LT1185 model an adequate surrogate.
Thank you.
The PSRR beyond 1MHz of LT1764A and LT1185 mainly depends on the parasitic, such as output capacitor, board layout....
For the 3rd rail, a LDO cannot generate a 5V output from a 5V input power supply.
adp1071 |
adp1071-1 |
adp1071-2 |
lt1020 |
lt1033 |
lt1083 |
lt1083-fixed |
lt1084 |
lt1084-fixed |
lt1085 |
lt1085-fixed |
lt1086 |
lt1087 |
lt1117 |
lt1118 |
lt1120 |
lt1120a |
lt1121 |
lt1123 |
lt1129 |
lt1175 |
lt117a |
lt117ahv |
lt1185 |
l… |
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |