The following circuit operates on the bench but isn't stable with a zero load (as shown: R8 is the output current sense resistor):
(Most components are as shown, but the FETs and the 2.5V references are different in the physical circuit, and the…
The following circuit operates on the bench but isn't stable with a zero load (as shown: R8 is the output current sense resistor):
(Most components are as shown, but the FETs and the 2.5V references are different in the physical circuit, and the…
With those small 100V transistors, I would not expect over 100W into 8 ohms (about +/-40V swing) and a couple slices to ease the heating. For 350W into 8 ohms, the swing is almost double that, so devices of at least 200V would be needed and 9A peaks, so…
Hi, Support Team
Regarding LT1166, I have the following questions, and could you give me some advice?
I want to design the parallel connection described in data sheet P14.
1.How do I determine the isolation inductor and small ballast resistor constants…
Hi All,
One of my customer made her schematic as attached.
- Part # : LT1166 (Power Output Stage Automatic Bias System)
The input voltage of this system is -8V ~ + 8V. (220Hz)
When this condition, customer want to get the output voltage of - 50V ~ + 50V. …
Hi All,
One of my customer made her schematic as attached.
- Part # : LT1166 (Power Output Stage Automatic Bias System)
The input voltage of this system is -6V ~ + 6V. (220Hz)
When this condition, customer want to get the output voltage of - 35V ~ + 35V…
The output devices will both be at quiescent setting when not delivering current to the load, but as one device delivers load current, the other device will be controlled to a lower current than quiescent, but not to zero current. If quiescent was set…
Hi all,
I have 2 questions for LT1166 when I reading the datasheet. hope someone really familiar with this IC can help me on this. really thanks a lot.
Q1:
what are the major differences between using LT1166 as current source drive and bipolar buffer…
The purpose of the LT1166 is specifically to prevent the non-linear cutoff of the classic class-B circuit by maintaining a continuous though reduced bias on the device not providing the load current. Look at the LTC6090 datasheet for an example.
你好,
我需要輸出+-60V/1Aout的1KHz Sine wave,所以選了ADHV4702-1加上LT1166來模擬,發現在一開始的時候,輸出端有個pulse出現,
於是參考ADHV4702-1 datasheet內的TYPICAL APPLICATION CIRCUIT 模擬,但是輸出總是會有一個pulse出現.
於是改成Unity-Gain Buffer,並且輸入端下地,依然輸出有一個pulse出現.
請問該如何解掉這根pulse呢?謝謝.