• RE: recommended bypass capacitor value for ada4522

    I have quiet power supplies (line transformer w/LT1086's). There is very little digital anywhere near the ada4522's, plus it is running on a separate power supply. The board will be shielded & filtered, so there is unlikely to be much RF present.…

  • AD8139 Not Working. I need help

    I am using the AD8139 in the as shown in the attached PDF.

    Spice simulations work fine. But On the bench using +-5V supplys,  AD8138 outputs Nothing.

    What did I do wrong.

    Stan Schekall a783239d66076ba983835f6e0157fe05.pdf

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • LT1074 output current

    Hey, I built a circuit as recommended in the datasheet, with R1 as pot to get variable output voltage. The problem I'm facing is I'm not getting load current more than 0.4A whereas the datasheet say it can output 5A. My output voltage drops if i increase…