请问LT1085可以直接用于负电压到负电压的转换吗?
目前的应用中需要7A的负电压输出,不过没找到大电流的负LDO,可以直接用正LDO来产生负电压吗?如何使用?
请问LT1085可以直接用于负电压到负电压的转换吗?
目前的应用中需要7A的负电压输出,不过没找到大电流的负LDO,可以直接用正LDO来产生负电压吗?如何使用?
I checked my history, and I don't have ESD data for the LT1085. You should be able to get that from ADI Technical Support on the ADI website.
adp1071 |
adp1071-1 |
adp1071-2 |
lt1020 |
lt1033 |
lt1083 |
lt1083-fixed |
lt1084 |
lt1084-fixed |
lt1085 |
lt1085-fixed |
lt1086 |
lt1087 |
lt1117 |
lt1118 |
lt1120 |
lt1120a |
lt1121 |
lt1123 |
lt1129 |
lt1175 |
lt117a |
lt117ahv |
lt1185 |
l… |
Device: LT1085IM
Vin = 9V
Vout = 5V
At -40C, the output of the LDO starts oscillating: Vin = 9V (green), Vout = 5V (Yellow), VADJ (orange)
Oscillation frequency = 2.9 MHz
Vout peak-to-peak oscillation = 1.2V
Two things fix the issue:
1) Lower the…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |
I am designing to different boards and each will have it's own 5V regulator on it but one will be higher current capable than the other. Signals from on board will be passed to the other board so the grounds will be tied together. Will this in effect…
Hey, I built a circuit as recommended in the datasheet, with R1 as pot to get variable output voltage. The problem I'm facing is I'm not getting load current more than 0.4A whereas the datasheet say it can output 5A. My output voltage drops if i increase…