• RH1056 (or LT1056) , maximum input current

    I am using the RH1056 as a transimpedance amplifier with a 50 MOhm feedback resistor.  Normally the currents from the photodiode connected to the RH1056 are low and the RH1056 does not saturate.

    I would like to know if the RH1056 inputs are clamped such…

  • RE: About the current boost amplifier using LT1010 (AN18)

    1. 18mA * 33Ohm = 594mV, so Q1 is on if 18 mA is flowing through 33Ohm (+15V to VCC). You mention that the output of LT1010 should be non-zero. Does this mean that the minimum output voltage of LT1010 should be at least 1.8V for turning on Q1? There is…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…