Hi Bram,
As far as I can see, LT1027 don't have package option on LS8, we only have SOIC and PDIP.
Regards,
Mon
Hi Bram,
As far as I can see, LT1027 don't have package option on LS8, we only have SOIC and PDIP.
Regards,
Mon
HI Vinayak Arkachari,
I would not recommend doing it in this design. Looking at the Absolute Maximum Rating, it can be seen that output to Ground Voltage should be limited to 7V but in this setup it will be -20V.
If you want to build a negative voltage…
Another option would be to use two MJE340's in a darlington pair configuration. This would increase HFE and decrease bias current errors. Alternatively, a high voltage MOSFET would also work. The amplifier you have looks fine. I'd go with an LT1027…
LT1460 |
LTC1258 |
LT1021 |
LT1027 |
LTC1798 |
RH1021-10 |
RH1021-5 |
RH1021-7 |
LT6660 |
LH0070 |
LTC6655 |
AD2700 |
AD2702 |
AD584S |
REF01S |
REF05S |
REF10S |
REF43S |
REF02S |
AD1582 |
AD1583 |
AD1584 |
AD1585 |
LT1019 |
LT1236 |
LTC6652 |
REF02… |
这是一个模拟世界。无论汽车、微波炉还是手机,所有电子设备都必须以某种方式与“真实”世界交互。为此,电子设备必须能够将真实世界的测量结果(速度、压力、长度、温度)映射到电子世界中的可测的量(电压)。当然,要测量电压,您需要一个衡量标准。该标准就是基准电压。
对系统设计人员而言,如何理解并使用何种基准电压源是很关键的~基准电压源旨在产生精确的电压,因此输出电压的数值和精度显然很重要。今天斑竹为大家带来了一份内部文档,帮助各位筒子们理解并使用基准电压源!
以及了解长期漂…
基准电压源是当代模拟集成电路极为重要的组成部分,它为串联型稳压电路、A/D和D/A转化器提供基准电压,也是大多数传感器的稳压供电电源或激励源,几乎在所有先进的电子产品中都可以找到。在近期的在线研讨会《电压基准源的产品及选择》中详细介绍了基准电压源的分类及工作原理和各类基准源的性能指标及主要的应用场合以及ADI的基准电压源的设计开发规划、产品优势以及对客户应用的价值所在。
本期研讨会的回放请点击:http://www.elecfans.com/d/908063.html
附件是本期研讨会的讲义,供大家下载并学习…