关于LT1019-5 DIP8 是否有可替代的料
Please provide the Dropout curve without normalization for the LT1019CS8-4.5. (Dropout vs load current)
Else, if the dropout curve is not available then please provide the values of dropout at any point.
Checking the datasheet of this product, it provides a list of suggested LTC Precision references. Looking at the the Reference design or the dev board DC1684A-B a 5V reference is used. I would like to know what exactly are the effects of using 10V reference…
Hi Santiago,
I sent your schematic around to a few people here, and they have some suggestions for you:
LT1460 |
LTC1258 |
LT1021 |
LT1027 |
LTC1798 |
RH1021-10 |
RH1021-5 |
RH1021-7 |
LT6660 |
LH0070 |
LTC6655 |
AD2700 |
AD2702 |
AD584S |
REF01S |
REF05S |
REF10S |
REF43S |
REF02S |
AD1582 |
AD1583 |
AD1584 |
AD1585 |
LT1019 |
LT1236 |
LTC6652 |
REF02… |
I've got myself an Eval-AD5781/91SDZ board (with an AD5791 onboard) and an SDP board for communicating with it over usb. Using the default jumper configurations, such that the positive and negative references are derived from a 5V reference input and…
Hi Reemo,
The ADN8810 is a 12-bit High Output Current source in which the output current is set by the below equation:
2f71b9506ce0d3ef470579daf13cc56d.html
The full scale current is dependent on the value of the sense resistors, R17_SPACER and R19_SPACER…