• Test Circuit for Offset Voltage on LT1006 spice model

    Test Circuit for Offset Voltage LT1006.asc

    Dear Support Team

    I drew the circuit that is on page 10 of the datasheet of LT1006 to measure offset voltage on LTSpice.

    I measured 628 uV of Offset voltage on output. 

    The first question I have is the following: Shouldn…

  • LTC6090 LT1006 LTC2057

    Hi,

    I have used these component to design a sinusoidal current generator 0-2Arms 50Hz-2kHz.

    I need to have a very low offset (DC component), max 300-400uA.

    Could you please give me help to low the offset?

    Thanks

    Best Regards

  • LTC6090 LT1006 LTC2057

    Hi,

    I have used these component to design a sinusoidal current generator 0-2Arms 50Hz-2kHz.

    I need to have a very low offset (DC component), max 300-400uA.

    Could you give me help to low the offset?

    Best Regards

  • LT1464 is there a flaw in the LTspice model?

    I am comparing Analog/Linear op amps (along with some by Brand X) using the NOISE analysis of LTspice. The context is: single supply via 9V battery, high source impedance, low bandwidth needed (-3dB at 20KHz would be fine). 

    When I test the LT1464 against…

  • Voltage-controlled current source

    Hello guys,


    I want to design voltage-controlled current source for my current project. The currents should be in a range from 0 to 2.5mA. Load resistance should be up to 5Kohm. My idea was to use unity gain amplifier together with the buffer in the configuration…

  • RE: Amplifiers for active electronic load

    Hi Tim,

    For the LT1006, I think the ADA4638-1 is an excellent part as replacement. ADA4638-1 is a high voltage, high precision, and zero-drift amplifier with rail-to-rail output. It has lower input offset voltage and drift, lower offset current, and…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • RE: Video DACs ADV7123-EP and ADV7393 output opamp driver circuit

    Attached is a app note on general video circuits including AC-coupling

      PDF

    For full galvanic isolation might be accomplished using video transformers however I do not have any experience with this path.  There are several transformer solutions used in…