Hi,
I am using this part in my design to get -2.5V but I am getting -4.2V.
The EN pin is connected to Vin. The input and output capacitors are Multilayer-ceramic 10uF one on each side. I applying -5V at Vin generated by LT1964ES5-5.
Can you please let…
I have two instances of LTC6600-2.5 in my circuit and the output voltage offset at U37 is about 55mV and at U36 is about 10mV.
what is the cause of output offset voltage difference?
How can I minimize the offset voltage at U36?
Here is my circuit(attach…
I Have a 1000M Enthernet Phy with 2.5 level the FPGA IO is fixed 1.8V . so need a level Translation chip for all TX/RX CLK
The clk up to 125Mbps . time rise 1ns.
could you please recommend one ?
Thank you very much.
Can you please…
I am performing a Pinsky Analysis to determine the risk of Tin Whiskers for the application we are utilizing the referenced component in. I need to know the plating process(electro-plated, immersion,etc) and the Tin plating thickness over the Leads.
The LT6600IS8-2.5 is a 2.2MHz differential lowpass filter so why are you using a 475MHz inputs signal?
Hello
Could ADPD188B support PM 2.5 detection? Thank you.
BR
Patrick
I need an accurate resistor with more than 256 Steps. Thats no problem by using the AD5248. I can connect the two potentiometer/ or rheostaten with some other resisors. I dont want describe the circuit i'm using more precisenlty.I'm interested in…
The answer might be too late for Tim, but others might face a similar problem.
If you change the output voltage by changing RSET, you also have to adjust the voltage divider from OUT to PGFB. If you don't do that, the startup circuit may try to quickly…
Hi Gaetano,
This is perfect, thanks.
2 layers can be difficult for routing. The VCC2P5 cap is particularly critical and doesn't have a great GND return path here due to routing being cut off on the bottom layer:
The red line shows the current shortest…