I'm interfacing the above device to an Xilinx Ultrascale+ FPGA.
Looking through the HMCAD1511 datasheet i cannot find any information on the setup and hold times with regards the LVDS output, this is needed for clock uncertainty.
Is there anymore…
I'm interfacing the above device to an Xilinx Ultrascale+ FPGA.
Looking through the HMCAD1511 datasheet i cannot find any information on the setup and hold times with regards the LVDS output, this is needed for clock uncertainty.
Is there anymore…
Hi,
1. When HMCAD1511 used as single channel mode, its maximum sample rate can be up to 1Gsps. If paralleling two HMCAD1511 together, is it possible to achieve 2Gsps? If possible, would you please promote a reference circuit?
2. For AD9094, there are…
Hi,
You're correct, the fs_ctrl registers finely adjusts the full-scale range for the analog inputs. The default full-scale range is 2Vpp. Therefore, an fs_ctrl<5:0>:00000 will correspond to 90% of the default full scale range, which is 1.8Vpp.…
Hi - In dual-channel operation, can the HMCAD1511 run directly off a 500MHz input clock for two-channels at 500MSPS? Or is the maximum sampling rate 250MSPS in this configuration?
For example: with 500MHz input clock, is clk_divide =1 and operating_mode…
Hi,
HMCAD1511 doesn't support trigger synchronization on-chip. You would need to perform the synchronization on the FPGA/ASIC side.
Regards,
Mark
Hi,
For better isolation, short the _P and _N pins of each analog input pair together. Place a 0.1uF capacitor to ground and connect the node to the Vcm pin of the HMCAD1511 with a 1k resistor.
Regards,
Mark
dear sir,
I found HMCAD1511 HMCAD1520 became “not recommend for new design” status, is there any replacement?
Will these two parts be end of life soon??
We just design a new product with HMCAD1511, we are very concerned about this status.
…Hi,
Did you purchase the eval kit for the hmcad1511, which includes the SP601? The eval kit comes with a CD installer for XIlinx ISE software.
Regards,
Mark
Hi all,
HMCAD1511/1520 input should be in the range 0V-2V, with an absolute rating -0.3V-2-3V according to datasheet.
Is there any clamping achieved in chip, or should we implement it with discrete components? If so, do you have any advises schematic…
Hello!
I purchased a HMCAD1511 board and wanted to evaluate it on a third-party XILINX SP605 development board.
But I only found hmc1520_sp601_rev118.mcs in the installation directory of the Easy suite,how can I get the mcs file for the SP605 board? and…