Hi,
Would like to request for the sequencing biasing for the hmc998apm5e. In addition, I would like to turn off the PA when it is not in use.
Hi,
Would like to request for the sequencing biasing for the hmc998apm5e. In addition, I would like to turn off the PA when it is not in use.
Hi,
Would like to check on the following.
1. Do I need to have decoupling capacitor on the Vdd?
2. What is the typical turn-on time of the hmc998?
Hi,
I have the following queries.
1. Can I request for the gain compression plot for 1GHz and also 6GHz,
2. Can I request for the OIP2 and OIP3 data when the amplifier is operating in saturation mode.
Hi,
Could I check what will be the harmonics performance when the amplifier is operating at saturation mode.
Hi ,
I have the following queries.
It would be of great help if you could kindly resolve the issue.
In the datasheet of HMC998APM5E at page 9 there is a graph "Second Harmonics vs Pout". I would like to know the effect of the same graph values if we…
Hello,
Can you please provide graph of MTBF as a function of Tj in hmc998apm5e MMIC?
Specifically i need the MTBF in Tj=205C
I know it's GaAs pHEMT, but i need to understand if in Tj=205C it will stop working or just deteriorate its performances.
Hi
Is there any data in using the HMC998APM5E for pulsed operation
I was thinking of using Vgg1 to turn on/off the amplifier, keeping Vdd and Vgg2 biased. The sequence would be similar to what AN1363 shows for the HMC637A. To turn off do in reverse.
1. Connect…
Hi,
I have two questions about the HMC998APM5E:
1.) I'd like to request a plot of Gain vs. Vgg1 for the HMC998APM5E (please). I'd received a similar set of gain plots for the HMC797, for Vgg=-6V, Vgg=-1V and Vgg=-2V from ADI, and assume the HMC998…
Hello! Excuse me, HMC998APM5E drain bias voltage is 15V power supply, how much is its external feed inductance? What is the bias resistance?