• HMC994 EVB thru loss and heat sink

    Hi folks,


    How could I get the thru loss about EVB of  HMC994 ?

    May you help to provide the relevant file to us for evaluate ?

    And I check the figure of  EVB board from website, here is a heat sink with screw, could you also provide related information…

  • RE: Cascading two HMC994 amplifiers with equalizers

    Hi Barath,

    Please check if all the components in your design are functional and have not sustained damage.
    The HMC994 is a wideband amplifier. Trace losses on the PCB can add up at higher frequencies. Please make sure you are deembedding the trace losses…

  • RE: Need for HMC907APM5E eval board gerber file

    Hello Dan02,

    If you investigate in excel file, the IC is HMC994 not HMC907. Also, the layout is compatible for HMC994. HMC907 has not either a VGG pin or a VDD pin. 

    Thanks,

  • RE: HMC797 Flat gain wideband amplifier

    Hi Jiamin,

    I would suggest the HMC998 as the closest possible replacement. The HMC994 is also similar but not as close as the HMC998 in my opinion.

    Thanks,

    DanO

  • RE: Query about powering HMC994LP5E

    HMC980 can be used to bias HMC994. HMC980 will generate the negative Vgate voltage and adjust Vgate continuously for constand Idd operation, and provide bias sequeuncing with additional features like short circuit protection.

    Best,

    Kagan

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description
  • 12/16/2015: Full RF Signal Chains from 0Hz to 110GHz

    Presenter: Mel Conway, Product Manager, Instrumentation, High-speed & RF and Precision

     

    This webcast will explain ADI's new and expanded RF capabilities since the acquisition Hittite Microwave. We will give examples of the wider frequency spectrum…

  • 【在线研讨会讲义PPT下载】从0Hz到110GHz的全频谱RF信号链

    此次在线研讨会阐释了自收购Hittite Microwave后ADI的全新及扩展的RF能力。我们会举例说明ADI涵盖的更宽频谱范围及其真DC的重要性。信号链外的性能同样至关重要,展示低噪声、高稳定性控制和电源元件如何改善总体RF信号性能,并将讨论完整的信号链示例。

    主要讨论天线到比特和比特到天线,信号链覆盖,即刚才提到的从真正的DC 0 Hz到110 GHz的频谱覆盖。 我会简要介绍其中涉及到的各类设备。

    为什么良好的RF需要良好的电源,大家知道,RF需要干净的电源。然后,最后会和大家讨论“不止是芯片…