• S-parameters for HMC941A.

    Please provide S-parameters for HMC941A. Thanks.

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • RE: HMC-ALH435-DIE 10 Ohms on Vgg1

    Hi avatar,

    1) It's in series of the path.

    2)  I would recommend a bondable resistor from AVX.

    3) The resistor in between the bypass capacitors is part of the noise filtering bypass circuit and also is there to protect the gate .

    Thanks,

    DanO

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…

  • HMC6981LS6 Die dimensions

    Hello,

    I am conducting thermal analyses in Ansys Icepak on a board with some HMC6981LS6 amplifiers on it.

    To properly model the amplifiers, I need to know the dimensions of the die, the die attach and the die pad, which I couldn't find on the datasheet…