• on/off time of ADRF5730 vs. HMC939ALP4E

    Hi,

     

    With past experience, GaAs parts’ switching speeds tend to increase by 100 to 200 ns at high temp. 

     

    For Silicon based parts, does the switching speed increase similarly as with GaAs parts?

  • HMC939ALP4E RF Port

    Hello,

    I would like to double check that the RF ports of HMC939ALP4E (RF1 & RF2) can be used in both directions. Can we get same performance when we use the pins in both direction?

    Best regards,

    Akira

  • PLEASE HELP!!! HMC939ALP4E is damaged when was turned on.

    What is the recommended power supply startup sequence?

    What happens if -5B is lost? or What happens if +5B is lost? or What happens if GND is lost?

    In all cases after the chip is damaged, the current in the -5V circuit is greater than 5 mA (25-100 mA…

  • RF amplitude settling time for 0.5 dB

    We are planning to use ADRF5731 and HMC939ALP4E. In the datasheet, RF amplitude settling time for 0.5 dB (50% triggered ctl to 0.5 dB of final RF output) is not mentioned. Can I get this data ?

  • HMC941ALP4E/HMC939ALP4E_Vdd Min and RF performance

    Dear team.

    customer is reviewing the HMC941ALP4E and HMC939ALP4E.

    1. Vdd +3.3V will be applied. is it possable?

    2. if +3.3V Vdd is applied,  is there any change in RF performance?

    3. Do you have a Min Vdd value?

    thanks,

    Best regards,

    Josh

  • RE: HMC939LP4E and HMC819LC5 not recommend

    Hello Ilke-san and Taz-san,

    Thank you for the reply.

    It is helpful if you send me the HMC939ALP4E preliminary datasheet.

    Regards,

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF