• HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Regarding HMC939A die. Do you have a calculated MTBF for this part available?

    MTBF or FIT per million hours needed to calculate my component MTBF

  • HMC939A

    Protection diodes shown on page 5 of data sheet: what type are these diodes?

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • ADSP-21483 Die temperature limits and accuracy

    Dear support team,

    I am currently measuring the 'Die' temperature of my DSP device.

    I was wondering, how accurate the measurement using the THD+ and THD- pins is and whether there are certain limits.

    At the moment, we analyze the DSP behaviour…

  • What is the best way to model HMC939A digital inputs for human body model class 3. I am using Spice to simulate my circuit.

    What is the best way to model the HMC939A digital inputs using spice?

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.