• HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • LT1764ADICE and LT1175-5DICE Die Composition and Bond Pad Metallization

    Hello,

    Please provide LT1764ADICE and LT1175-5DICE Die Composition and Bond Pad Metallization. I am unable to locate this information.

    Thank you in advance,

    StoneOLD

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…

  • HMC6981LS6 Die dimensions

    Hello,

    I am conducting thermal analyses in Ansys Icepak on a board with some HMC6981LS6 amplifiers on it.

    To properly model the amplifiers, I need to know the dimensions of the die, the die attach and the die pad, which I couldn't find on the datasheet…

  • AD8515: Die size

    Are these dies AD8515 and OP284CHIPS smaller than 1 x 1 mm²? That would be an
    absolute max for us.

     

    1. The OP284CHIPS has a die size of 1.620 mm x 2.301 mm.
    2. The AD8515 has a die size of 0.660 mm x 0.920 mm.

    Therefore only the…
  • ADG5206 bare die

    Hi,

    Currently we are using ADG5206 (LFCSP_WQ package) and we are looking for ways to decrease the required footprint per channel. One way would be using bare dies. As there is a list of "as bare die" available products ( http://www.analog.com…

  • AD8354 bare die

    Hello,

    Do you sell this amplifier as a bare die,  without the package?

     Thank you in advance,

  • AD2428WCCSZxx die revision

    Hi

    Could you kindly let us know what difference with AD2428WCCSZ and AD2428WCCSZ01?

    Our customer use AD2428WCCSZ01 first, but they want to modify to non-automotive version, but AD2428BCPZ no die revision, they confuse about it.

  • AD825 die backside connection

    I have no indication on Backside connection.
    Which potential should I connect the backside of the AD825 die?

     

    You should not connect die backside. Please let die backside float.