• HMC930A

    Hello,

    I'd like to request the data presented in the datasheet in Excel file format. Specifically, I'd like to request S-Parameter data for the HMC930A. To include graphed data if available, preferably in Excel Format for the following:

    P1dB…

  • HMC930A power dissipation

        Hello, dear colleagues!

    Could You clear, if HMC930A can work with +7 V supply?

    What power dissipation will be in this case,

    and what NF can we expect,

    if amlifier was tested in that condition (+7 V voltage)?

    Thanks!

    Regards,

    K.

  • Gain and Return Loss - HMC930A

    About HMC930A. Is the gain stated in the datasheet the effective gain or should I subtract from it the losses due to return loss? For example, if I am inserting a power of 10dBm to the HMC930A, is the output about 20dBm or would it be less due to the…

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.