• HMC910 / HMC911: has anyone notiched that the input impedance for these chips was changed from 75 to 50Ohm?

    HMC910 / HMC911: has anyone notiched that the input impedance for these chips was changed from 75 to 50Ohm?

  • Inquiry for specification of time delay device

    I found 'Delay Control Modulation Bandwidth' specification in HMC910 datasheet.

    But, I can not understand meaning of 'Delay Control Modulation Bandwidth'

    Please, explain meaning of 'Delay Control Modulation Bandwidth'.

    Delay…

  • RE: Refection in REFA of AD9525

    pkern:

    Maybe I find the reason for the reflection. I use HMC910 in previous of AD9525. Each pin of output diff. driver of HMC910 is connected to VCC via a 50 ohm resister, as the picture below shows. So the differential impedance between of QN and QP…

  • RE: AD9854 Synchronization Questions

    Hi Evan,

     

    Here are the list of available D flip-flops that are available on the Analog Website.

     

    Part Number

    Product Description

    High Speed Logic Function

    Data Rate (max)

    Clock Input (max)

    Output Fall Time (typ)

    Output Rise Time (typ)