• HMC907 Power Supply connection.

    Hello, 

    Datasheet for HMC907 says that pin №21 is RF output for amplifier and connect DC bias (Vdd) network to provide drain current (Idd). Also Drain Bias (Vdd) must be applied through a broadband bias tee or external bias network. And there are only 2…

  • RE: HMC907 IP3 at low frequencies

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: The worst VSWR for the HMC907 output port

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Need help with HMC907 EVB Gerber

    Dear Sir,

    Could you provide HMC907LP5E EVB  Gerber File to me for a reference?

     

    Thanks!

  • 一般power amplifier的输出驻波可接受的最差值(如HMC907)是多少

    为了避免回波造成的PA烧毁,一般PA输出端连接负载的端口驻波最差情况下可以是多少

  • RE: HMC 907 Bias Tee

    Hi,

    I read that article, thank you.

    I would like to use the Coilcraft 0402DF-560 XJR inductor, for both HMC797 and HMC907, do you think it could work?

  • RE: Need for HMC907APM5E eval board gerber file

    Hello Dan02,

    If you investigate in excel file, the IC is HMC994 not HMC907. Also, the layout is compatible for HMC994. HMC907 has not either a VGG pin or a VDD pin. 

    Thanks,

  • HMC907APM5E thermal impedance

    I have been looking at using a HMC907APM5E and HMC998APM5E power amplifier in our application and had a question about thermal impedance specifications from the datasheets for these parts. For the HMC907 i am seeing 16.7°C/W for thermal impedance specified…

  • RE: Packaged Part Numbers

    Hello Jetheo,

    The HMC913 SDLVA design has two product pages with separate datasheets on the website. For bare die, simply order HMC913 (no suffix). Orders with the suffix LC4B would indicate the ceramic packaged part. 

    Schematic of the packaged part demo…

  • RE: ADF5355 RFOUT B AC or DC coupled

    Hi eTa,

    I support the HMC606LC5 and HMC907LP5E so I will comment with respect to your questions about those products. I'd like to mention that the HMC907LP5E is obsolete and no longer available, but its successor product the HMC907APM5E should soon become…