• layout pattern for hmc715lp3e ,hmc547lp3 ,HMC902LP3E,HMC451LP3E 

    hi i need .bxl or pcb layout for hmc715lp3e and hmc547lp3 and HMC902LP3E and HMC451LP3E but can not find it on ultra librarian. i emailed  Package.Wizard@analog.com but could not get these layout . is there any pattern suggested for these parts?

  • hmc902LP3E的第14引脚怎么时接地的啊?

    在测试芯片引脚时,发现hmc902LP3E的电源引脚是接地的,麻烦问一下是本来就接地还是其他可能原因?谢谢

  • RE: MTBF data request

    Hi Sir,

    Please share the MTBF result of the remaining IC's,

    HMC8411LP2FE
    HMC3653LP3BE
    HMC902LP3E
    HMC787ALC3B

  • HMC902LP3E_ESD level

    Hello Team,

    Could I know the ESD level for HMC902LP3E?

    - HBM

    - CDM

    - MM

    Thank you

    Regards,

    Josh

  • MSL rating of HMC902 & HMC903?

    Hi

    What is the MSL rating of HMC902LP3E and HMC903LP3E? I can't find the MSL rating in the datasheets, and the parts do not have Material Declaration documents on the website.

  • HMC902LP3 Biasing

    Hello,

    I intend to use HMC902LP3E with self-bias configuration (i.e. Vgg1,2 = 0V). Could you confirm that I can use the following Turn ON/OFF procedure:

    Turn ON:

    1. Set Vgg1,2 and Vdd1,2 to 0 V
    2. Set Vdd1,2 to 3.5 V

    3. Apply RF power


    Turn OFF:
    1.…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description
  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF