• RE: usage of HMC892A

    Hi Ma Yugang,

    Apologies for the delayed response on this inquiry, as I missed during the holiday season. Yes, the HMC892A insertion loss can vary from -13 to -7dB depending upon the frequency of operation. Typically these tunable filters are placed after…

  • RE: Analog Band Pass Tunable Filters (ADMV8420,ADMV8416,HMC892A,HMC891A)

    Hi, Thats a nice result. Could you inform me what OPamp feedback you use here?

    Thanks

  • Tunable Band-Pass Filter HMC892A

    Hello! I need a detailed frequency response in the range 5470-5610 MHz tunable Band-Pass Filter HMC892A

  • RE: RFPD-RC-4450-50 interface to ADRV9002

    Yes but you will need to make sure the RFPD-RC-4450-50 is configured properly first.  The first decision is whether to include the HMC892A in the receive chain.  If you do, C76, C203, and C211 need to be not populated.  C212 and C75 need to be populated…

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF